DOCA0221EN-01

Fixed ComPacT NS630b-1600 with Direct Rotary Handle

Fixed Device with Direct Rotary Handle

  1. Arc chute

  2. MicroLogic trip unit

  3. Front cover

  4. Direct rotary handle

  5. Rating plate

  6. Slot for optional keylock

  7. Push-to-trip button

  8. QR code on MicroLogic trip unit

For detailed information about mounting a fixed ComPacT NS630b-1600 with direct rotary handle, see JYT6180003 ComPacT NS630b-1600 - Fixed Circuit Breaker or Switch-Disconnector - Instruction Sheet.

For detailed information about mounting a direct rotary handle on a fixed ComPacT NS630b-1600, see BQT1167502 ComPacT NS630b-1600 - Direct Mounted Rotary Handle - Instruction Sheet.

Accessories for Fixed Device with Direct Rotary Handle

  1. Brackets for horizontal mounting

  2. Carrying grip

  3. BCM ULP communication module

  4. OF1 ON/OFF indication auxiliary (wired or wireless)

  5. OF2 ON/OFF indication auxiliary (wired or wireless)

  6. OF3 ON/OFF indication auxiliary (wired or wireless)

  7. SD trip-indication auxiliary (wired or wireless)

  8. MX opening voltage release or MN undervoltage release

  9. SDE fault-trip indication auxiliary (wired or wireless)

    Zoom Z1

  10. Control auxiliary terminals

  11. CAO1 early-break contact

  12. CAO2 early-break contact

  13. CAF1 early-make contact

  14. CAF2 early-make contact

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.