DOCA0221EN-01

Routine End-User Preventive Maintenance Program (Yearly)

Minor preventive maintenance operations such as greasing and operating checks, as well as repairs by standard exchange of certain assemblies, carried out by a certified customer employee according to the manufacturer maintenance instructions.

Part

Procedure title

Year

Tool

1 2 3 4

5*

Device

Check the general condition of the device (escutcheon, case, chassis, connections, terminal shields).

None

Mechanism

Open/close device manually.

None

Check complete closing of device poles.

None

Check number of device operating cycles.

Operation counter

Breaking unit

Check the cleanliness of the filters.

None

Control auxiliaries (electrical operated device)

Check auxiliary wiring and insulation.

None

Device locking

Open and close keylocks installed on device.

None

Open and close padlocking system installed on device.

None

Chassis (optional)

Remove device from chassis and put it back.

None

Check operation of position contacts (CE, CT, CD).

None

Check operation of safety shutters.

None

Chassis locking (optional)

Open and close keylocks installed on chassis.

None

Operate padlocking system.

None

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.