DOCA0221EN-01

Matching a Device With its Chassis

The optional mismatch protection helps to ensure that the moving part of the device is installed only in a chassis with compatible characteristics. The possible combinations are listed below.

A B C

4 5

B C D

1 5

A B D

3 5

B C E

1 4

A B E

3 4

B C

1 4 5

A B

3 4 5

B D E

1 3

A C D

2 5

B D

1 3 5

A C E

2 4

B E

1 3 4

A C

2 4 5

C D E

1 2

A D E

2 3

C D

1 2 5

A D

2 3 5

C E

1 2 4

A E

2 3 4

D E

1 2 3

To set up a mismatch prevention combination for the device and the chassis, consult the instruction sheet on the Schneider Electric website: 51201012AA.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.