DOCA0221EN-01

Greasing

Do not use too much grease. When excess grease mixes with dust it can affect the mechanism operation.

Greasing must be done after cleaning of some mechanical parts as described in the maintenance procedures. Use only grease recommended by Schneider Electric.

The main contacts must not be greased.

Under normal operating conditions, the pole-operating mechanism does not need to be regreased (greased for the life of the product).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.