DOCA0221EN-01

Harsh Conditions and Device Not Installed Inside a Switchboard

The time interval between two preventive maintenance visits must be reduced by half if any of the conditions presented below are present.

Harsh operating and environmental conditions

Temperature (annual average)

Average annual temperature around the switchboard: 35 °C to 45°C (95 °F to 113°F) (Ti*)

Percent load

> 80% of In 8/24 hours or 24/24 hours

Relative humidity

> 80%

Corrosive atmosphere

Device installed in environment category 3C3 or 3C4 without any particular protection

Salt environment

Installation < 10 kilometers from seaside and device without any particular protection

Dust

High level

Device not installed inside an enclosure equipped with filters or a ventilated IP54 enclosure

Vibration

Continuous vibrations between 0.2 g (0,007 oz) and 0.5 g (0,018 oz)

Example depending on the conditions:

  • Normal: check on charging time = every 2 years

  • Harsh: check on charging time = 0.5 x 2 = 1 (every year)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.