DOCA0221EN-01

Auxiliary Wiring

Auxiliary wiring is used to transmit the following information:

  • Orders to the control devices

  • Status condition information

Incorrect connections or damaged insulation can cause unexpected opening or non-operation of the device. The auxiliary wiring must be regularly inspected and replaced as required, particularly in environments with vibrations, high ambient temperatures, or corrosive atmosphere.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.