DOCA0221EN-01

Withdrawable ComPacT NS630b-1600 with Toggle Handle

Withdrawable Device Moving Part with Toggle Handle

  1. Mounting side plates

  2. Carrying grip

  3. Arc chute

  4. MicroLogic trip unit

  5. Front cover

  6. Rating plate

  7. Fixed padlocking device for toggle handle locking in ON or OFF positions (optional)

  8. Removable padlocking device for toggle handle locking in OFF position (optional)

  9. Toggle extension (optional)

  10. Toggle handle

  11. Device rating

  12. Push-to-trip button

  13. QR code on MicroLogic trip unit

For detailed information about mounting a withdrawable ComPacT NS630b-1600 with toggle handle, see JYT6180103 ComPacT NS630b-1600 - Withdrawable Circuit Breaker or Switch-Disconnector - Instruction Sheet.

Accessories for Withdrawable Device with Toggle Handle

  1. Mismatch protection

  2. BCM ULP communication module

  3. Disconnectable contact block

  4. OF1 ON/OFF indication auxiliary (wired or wireless)

  5. OF2 ON/OFF indication auxiliary (wired or wireless)

  6. OF3 ON/OFF indication auxiliary (wired or wireless)

  7. SD trip-indication auxiliary (wired or wireless)

  8. MX opening voltage release or MN undervoltage release

  9. SDE fault-trip indication auxiliary (wired or wireless)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.