DOCA0221EN-01

Locking Using One to Three Padlocks

Use padlocks with a shackle diameter of 5 to 8 mm (0.2 to 0.3 in).

Step

Action

1

Device in disconnected position.

2

Pull out the tab.

3

Insert the shackle (diameter 5 to 8 mm (0.2 to 0.3 in)) of the padlock(s).

NOTE: Padlocks are not supplied.

4

The racking handle cannot be inserted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.