DOCA0221EN-01

Removing the Withdrawable Device

Device Removal

NOTICE
HAZARD OF EQUIPMENT DAMAGE
The chassis must be securely fastened when installing or removing the device.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

Put the device in the open position.

2

Pull out the rails in the chassis until they are fully extended.

3

Pull out the device to the maximum in the chassis by rolling it along the rails.

Result: The device is supported on the rails, clear of the chassis and ready to be lifted.

Lifting the Device

Both the device and chassis have a carrying grip for lifting. To lift the device, use an overhead lifting device attached to the carrying grip, following the directions given in this section.

DANGER
HAZARD OF DEVICE FALLING
  • Be sure that lifting equipment has lifting capacity for the device being lifted.
  • Follow manufacturer’s instructions for use of lifting equipment.
  • Wear hard hat, safety shoes, and heavy gloves.
Failure to follow these instructions will result in death or serious injury.

Lift the device from the chassis rails by using the carrying grip located on the sides of the device.

Device Weights

Number of poles Device Weight (kg)

3P

Moving part (Withdrawable)

14

Chassis

16

Fixed device

14

4P

Moving part (Withdrawable)

18

Chassis

21

Fixed device

18

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.