DOCA0221EN-01

Opening and Closing Cycles

The need to ensure continuity of service in an installation generally means that power devices are rarely operated. An excessive number of operating cycles accelerates aging and a lack of operation over a long period can result in mechanical malfunctions. Regular operation is required to maintain the normal performance level of all parts involved in the opening and closing cycles.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.