DOCA0221EN-01

Manufacturer Preventive Maintenance Program (Every 5 Years)

All major preventive and corrective maintenance work carried out by the Schneider Electric after-sales support department.

Part

Procedure title

Year

Tool

5 10 15 20 25
Case

Measure insulation resistance.

Ohmmeter

Breaking unit

Measure the voltage drop across main contacts for each pole.

Ohmmeter + Injection unit

Control auxiliaries

Preventive replacement of control auxiliaries.*

None

MicroLogic trip unit

MicroLogic replacement.*

None

Check DIN/DINF tripping using performer test tool.

Performer test kit

Chassis (optional)

Check connection/disconnection torque.

Dynamometric crank

Communication module and accessories

Test the device control, the uploading of contact status (OF, SD, SDE) operation of optical link, by using the communication network.

Service Interface+ EcoStruxure Power Commission software

Test by using the communication network:

  • Uploading of chassis position contacts

    .
  • Synchronisation of the address between BCM ULP and IO module

    .
  • Forced replication of the BCM address.

Service Interface+ EcoStruxure Power Commission software

Test the writing of data into MicroLogic by using the communication network.

Service Interface+ EcoStruxure Power Commission software

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.