DOCA0221EN-01

Racking-out the Device From Connected to Test Position

Step

Action

1

Remove the racking handle from its storage space.

2

Insert the racking handle into the racking handle slot.

3

Push in the position release button.

4

Turn the racking handle counterclockwise.

Result: The device moves forward in the chassis.

5

When the test position is reached, the position release button pops out and the mechanism blocks the racking handle.

Result: The device is in the test position. Remove the racking handle or continue to disconnected position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.