DOCA0221EN-01

Racking-in the Device From the Test to Connected Position

Step

Action

1

The device is in test position. Push in the position release button.

2

Turn the racking handle clockwise.

Result: The device moves back in the chassis.

3

When the connected position is reached, the position release button pops out and the mechanism blocks the racking handle.

Result: The device is in the connected position.

4

Remove the racking handle from the racking slot.

5

Put the racking handle back into its storage space.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.