DOCA0221EN-01

Fixed ComPacT NS630b-1600 with Toggle Handle

Fixed Device with Toggle Handle

  1. Arc chute

  2. MicroLogic trip unit

  3. Front cover

  4. Rating plate

  5. Fixed padlocking device for toggle handle locking in ON or OFF positions (optional)

  6. Removable padlocking device for toggle handle locking in OFF position (optional)

  7. Toggle extension (optional)

  8. Toggle handle

  9. Device rating

  10. Push-to-trip button

  11. QR code on MicroLogic trip unit

For detailed information about mounting a fixed ComPacT NS630b-1600 with toggle handle, see JYT6180003 ComPacT NS630b-1600 - Fixed Circuit Breaker or Switch-Disconnector - Instruction Sheet.

Accessories for Fixed Device with Toggle Handle

  1. Brackets for horizontal mounting

  2. Carrying grip

  3. BCM ULP communication module

  4. Control auxiliary terminals

  5. OF1 ON/OFF indication auxiliary (wired or wireless)

  6. OF2 ON/OFF indication auxiliary (wired or wireless)

  7. OF3 ON/OFF indication auxiliary (wired or wireless)

  8. SD trip-indication auxiliary (wired or wireless)

  9. MX opening voltage release or MN undervoltage release

  10. SDE fault-trip indication auxiliary (wired or wireless)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.