DOCA0221EN-01

Locking the Safety Shutters

The following illustrations show the four locking possibilities inside the chassis using one or two padlocks (shackle diameter 5 to 8 mm (0.2 to 0.3 in)) for each shutter.

Top and bottom shutters not locked.

Top shutter not locked.
Bottom shutter locked.

Top shutter locked.
Bottom shutter not locked.

Top and bottom shutters locked.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: 51201011AA.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.