DOCA0221EN-01

Racking-out the Device From Test to Disconnected Position

Step

Action

1

Push in the position release button.

2

Turn the racking handle counterclockwise.

Result: The device moves forward in the chassis.

3

When the disconnected position is reached, the position release button pops out and the mechanism blocks the racking handle.

Result: The device is in the disconnected position.

4

Remove the racking handle from the racking slot.

5

Put the racking handle back into its storage space.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.