DOCA0221EN-01

Device Identification

Rating Plate

  1. Performance level

  2. ComPacT NS type and rated current

  3. Ui: rated insulation voltage

  4. Ue: rated operational voltage

  5. Icw: rated short-time withstand current

  6. Frequency

  7. Standard

  8. Type of device: circuit breaker or switch-disconnector

  9. Uimp: rated impulse withstand voltage

  10. Ics: rated service short-circuit breaking capacity

  11. Icu: rated ultimate short-circuit breaking capacity

  12. Not applicable for IT networks

  13. Selectivity category as per IEC 60947-2

QR Code

When the QR code on the front face of a MicroLogic trip unit is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed. The landing page displays some information about the device and a list of menus (see detailed topic).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.