DOCA0221EN-01

Power Connections

WARNING
HAZARD OF EQUIPMENT DAMAGE AND THERMAL RUNAWAY
Do not use a combination of different materials for connections (for example, copper and aluminium).
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Power connections between the various distribution systems in a switchboard (busbars, cables) and the switchgear are a major source of heat loss.

Incorrect tightening can cause thermal runaway, which in turn can damage the device or cable insulation and can cause a short-circuit and even a fire. Damage can be due to disregard for installation requirements during switchboard assembly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.