DOCA0221EN-01

Fixed ComPacT NS1600b-3200 Description

Device Description

  1. Arc chute

  2. Front cover

  3. Rating plate

  4. Fixed padlocking device for toggle handle locking in ON and OFF positions (optional)

  5. Removable padlocking device for toggle handle locking in OFF position (optional)

  6. Toggle handle

  7. Push-to-trip button

  8. QR code on MicroLogic trip unit

  9. MicroLogic trip unit

For detailed information about mounting a fixed ComPacT NS1600b-3200, see JYT6180203 ComPacT NS1600b-3200 - Fixed Circuit Breaker or Switch-Disconnector - Instruction Sheet.

Device Accessories

  1. BCM ULP communication module

  2. Control auxiliary terminals

  3. OF1 ON/OFF indication auxiliary (wired or wireless)

  4. OF2 ON/OFF indication auxiliary (wired or wireless)

  5. OF3 ON/OFF indication auxiliary (wired or wireless)

  6. SD trip-indication auxiliary (wired or wireless)

  7. MX opening voltage release or MN undervoltage release

  8. SDE fault-trip indication auxiliary (wired or wireless)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.