DOCA0221EN-01

Indication Contacts

Introduction

One indication contact model provides OF, SD, SDE, CAO and CAF indication functions. The position of the contact inside the case determines the function.

Indication contacts are under the front face of the circuit breaker. Installation is in a compartment isolated from the power circuits. There are two types:

  • Standard contact with spring terminals

  • Low-level contact with screw terminals

For more information about installation, consult the instruction sheet on the Schneider Electric website: NNZ4314501.

Standard and Low-Level Contacts

Standard and low-level contacts are the common point changeover type.

NC Normally Closed contact

NO Normally Open contact

The following table describes the operation of standard and low-level volt-free contacts:

Name

Definition

OF indication contact

Changeover: The NO contact is normally open when the circuit breaker is in the O (OFF) position.

SD indication contact

Trip indication: The SD contact indicates that the circuit breaker has tripped due to:

  • Instantaneous protection

  • Long-time protection

  • Short-time protection

  • Ground-fault protection

  • Earth-leakage protection

  • Operation of the MX or MN voltage releases

  • Operation of the push-to-trip button

  • Connecting/Disconnecting the withdrawable circuit breaker

SDE indication contact

Electrical fault indication: The SDE contact indicates that the circuit breaker has tripped on an electrical fault due to:

  • Instantaneous protection

  • Long-time protection

  • Short-time protection

  • Ground-fault protection

  • Earth-leakage protection

CAO early-break contact

Rotary handle position indication: The CAO early-break contact indicates that the rotary handle started to turn to the open position.

CAF early-make contact

Rotary handle position indication: The CAF early-make contact indicates that the rotary handle started to turn to the closed position.

Operation of the Indication Contacts

The following figures show the position of the indication contacts for each position of the operation handle and main contacts.

Name

Contact number

Position of the operation handle and contacts

Toggle handle position

Rotary handle position

Device status

OFF

ON

Tripped (by MicroLogic trip unit)

Tripped by MN/MX or push-to-trip

Tripped by protection

Main contact position

Open

Closed

Open

Open

Open

OF indication contact position

1–2

Closed

Open

Closed

Closed

Closed

1–4

Open

Closed

Open

Open

Open

SD indication contact position

1–2

Closed

Closed

Open

Open

Open

1–4

Open

Open

Closed

Closed

Closed

SDE indication contact position

1–2

Closed

Closed

Open

Closed

Open

1–4

Open

Open

Closed

Open

Closed

Operation of Early-Break and Early-Make Contacts

A change in position of the direct and extended rotary handles is indicated by the following early-break and early-make contacts:

  • CAO: early-break contact indicates that the rotary handle started to turn to the open position. It can be used to open the contactor control circuit before the circuit breaker opens.

  • CAF: early-make contact indicates that the rotary handle started to turn to the closed position. It can be used to supply an MN undervoltage release before the circuit breaker closes.

Name

Contact number

Position of the operation handle and contacts

Rotary handle position

Main contact position

Open

Open

Closed

Closed

Open

CAO early-break contact

1–2

Open

Closed

Closed

Open

Open

1–4

Closed

Open

Open

Closed

Closed

CAF early-make contact

1–2

Closed

Open

Open

Closed

Closed

1–4

Open

Closed

Closed

Open

Open

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.