DOCA0221EN-01

Chassis for Withdrawable ComPacT NS630b-1600 Device

The chassis is identical for withdrawable ComPacT NS630b-1600 devices with:

Chassis

  1. Carrying grip

  2. Arc chute cover

  3. Terminal blocks for accessories

  4. Terminal block identification plate

  5. Chassis locking by padlocks

  6. Moving part position indicator (connected, test, or disconnected)

  7. Racking handle socket

  8. Position release button

  9. Racking handle storage

  10. Racking handle

  11. Withdraw grip

  12. Extension rail

  13. Top safety shutters

  14. Bottom safety shutters

Chassis Accessories

  1. Door interlock

  2. Mismatch protection

  3. Withdrawable device position contacts

  4. Terminal blocks for optional accessories

  5. Chassis locking by keylocks

  6. Open-door racking interlock

  7. Auxiliary terminal shield

Chassis Terminal Block

The following example shows a withdrawable device with toggle handle. The terminal blocks are identical for devices with direct rotary handle and extended rotary handle.

Assignment of Chassis Terminal Blocks

The following table describes the assignment of the terminal blocks for withdrawable circuit breakers and switch-disconnectors:

  • Optional terminal blocks are delivered on the chassis only if the associated optional accessories are installed in the device.

  • N/A indicates that the terminal blocks and the associated optional accessories are not compatible with the device.

Block

Marking

Description

Circuit breaker

Switch-disconnector

A

CD1-CD2

2 CD disconnected position contacts

Optional

Optional

B

Com

Terminal block for the BCM ULP communication module

Optional

N/A

UC1

Zone selective interlocking (ZSI), rectangular sensor for earth-leakage protection, or MDGF module input

  • Standard with MicroLogic A/E/P trip units

  • N/A with MicroLogic trip units without measurements

N/A

UC2

Neutral external sensor, rectangular sensor for earth-leakage protection, or MDGF module input

N/A

UC3

External 24 Vdc power supply and external voltage

N/A

CAF1-CAF2

Early-make contact (rotary handle)

Optional

Optional

SDE

SDE fault-trip indication contact

Optional

N/A

MN/MX

MN undervoltage release

or MX opening voltage release

Optional

Optional

MT1

Electrical closing order

N/A

N/A

MT2

Electrical opening order

N/A

N/A

SD

Trip indication contact

Optional

Optional

CAO1–CAO2

Early-break contact (rotary handle)

Optional

Optional

OF1-OF3

3 OF indication contacts

Optional

Optional

C

CE1–CE3

3 CE connected position contacts

Optional

Optional

CT1

1 CT test position contact

Optional

Optional

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.