DOCA0221EN-01

Withdrawable ComPacT NS630b-1600 with Extended Rotary Handle

Withdrawable Device Moving Part with Extended Rotary Handle

  1. Mounting side plates

  2. Carrying grip

  3. Arc chute

  4. MicroLogic trip unit

  5. Front cover

  6. Telescopic shaft

  7. Extended rotary handle

  8. Rating plate

  9. Slot for optional keylock

  10. Push-to-trip button

  11. QR code on MicroLogic trip unit

For detailed information about mounting a withdrawable ComPacT NS630b-1600 with extended rotary handle, see JYT6180103 ComPacT NS630b-1600 - Withdrawable Circuit Breaker or Switch-Disconnector - Instruction Sheet.

For detailed information about mounting an extended rotary handle on a withdrawable ComPacT NS630b-1600, see BQT1167602 ComPacT NS630b-1600 - Extended Rotary Handle - Instruction Sheet.

Accessories for Withdrawable Device with Extended Rotary Handle

  1. Mismatch protection

  2. BCM ULP communication module

  3. Disconnectable contact block

  4. OF1 ON/OFF indication auxiliary (wired or wireless)

  5. OF2 ON/OFF indication auxiliary (wired or wireless)

  6. OF3 ON/OFF indication auxiliary (wired or wireless)

  7. SD trip-indication auxiliary (wired or wireless)

  8. MX opening voltage release or MN undervoltage release

  9. SDE fault-trip indication auxiliary (wired or wireless)

    Zoom Z1

  10. CAO1 early-break contact

  11. CAO2 early-break contact

  12. CAF1 early-make contact

  13. CAF2 early-make contact

The chassis is identical for all withdrawable ComPacT NS630b-1600 devices. For more information about the chassis and its mismatch protection, see Chassis.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.