EIO0000005608.01

RS-422/485 端口设置

切换 RS-422 和 RS-485时,请遵循以下步骤。
  1. 显示BIOS屏幕。请参阅 Harmony PSA6 Windows System Setting User Guide
  2. 选择 Advanced > NCT5525D Super IO Configuration > Serial Port 2 Configuration
  3. 选择 COM port 2 Mode
  4. 选择 RS-422RS-485
  5. 按 [F4] 键。
  6. Save & Exit Setup(保存并退出设置)对话框中选择 Yes(是)。
  7. 产品重新启动。
反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.