DOCA0272EN-00

Configure TeSys™ island as a Bus Device

The TeSys™ island bus coupler must be configured before it can be used as a bus device in combination with a Siemens® CPU. The following procedures describe the steps necessary to configure the TeSys island as a bus device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.