DOCA0272EN-00

UDT_PVControl

The PVControl UDT is used to transfer an avatar’s cyclic process variable data, like analog values from sensors and discrete signals from switches. The interfaces of the PROFINET IO and PROFIBUS DP application avatar function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

PVInput0

INT

Process variable input for analog value

PVInput1

INT

Process variable input for analog value

PVInput2

INT

Process variable input for analog value

PVInput3

INT

Process variable input for analog value

PVInput4

INT

Process variable input for analog value

PVSwitch0

BOOL

Process variable switch for discrete signals

PVSwitch1

BOOL

Process variable switch for discrete signals

PVSwitch2

BOOL

Process variable switch for discrete signals

PVSwitch3

BOOL

Process variable switch for discrete signals

PVSwitch4

BOOL

Process variable switch for discrete signals

Reserve

BOOL

 

Reserve

BOOL

 

Reserve

BOOL

 

PVControlIn0

BOOL

Status of PV Control-Input 0

PVControlIn1

BOOL

Status of PV Control-Input 1

Reserve

BOOL

 

Reserve

BOOL

 

Reserve

BOOL

 

Reserve

BOOL

 

Reserve

BOOL

 

Reserve

BOOL

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.