DOCA0272EN-00

UDT_RDREC

The RDREC UDT is used to store status information of an acyclic read request internally.

Elements

Element

Data Type

Description

xQ_RTrig

BOOL

Rising edge result, to transfer data to function block variables

qxValid

BOOL

Acyclic read request result is VALID

qxBusy

BOOL

Acyclic read function is busy

qxError

BOOL

Acyclic read request ends with ERROR

qdwStatus

DWORD

Status result of acyclic read function

quiLen

UINT

Length of read data as feedback value.

ixStartRead

BOOL

Enable/Start acyclic read function

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.