DOCA0272EN-00

Switch – SIL Stop, W. Cat. 3/4

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 3 and Category 4 according to ISO 13849.

Function block profile

Function block type

Avatar Control function block.

Type of data access

Cyclic (read/write) and acyclic (read).

Intended use

Device avatar “Switch – SIL Stop, W. Cat. 3/4”

Functionality

The Switch SIL Stop Cat function block establishes or interrupts a power line in an electric circuit with Stop Category 0 or Stop Category 1*, Wiring Category 3 and Category 4.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.