DOCA0272EN-00

Integrating the Function Block Library

To integrate the IEC 61131-3 function block library file for the TeSys island PROFINET IO and PROFIBUS DP bus couplers, download the file from https://www.se.com/ww/en/product-range-download/65746-tesys-island/.

Use the following steps to install the file in Siemens TIA Portal after you download the file:

  1. Launch Siemens TIA Portal, then click Project View.

  2. Select Global libraries → Retrieve library in the Options menu, then click Ok.

    Retrieve Library

  3. Select the archive file of the function block library you downloaded.

  4. Click Open, then select the Automation directory as the target directory.

  5. Click OK.

    Automation Directory

  6. The following Open library window might display prompting you that the library version will be upgraded to version 15.1, depending on the version of TIA Portal that you are using.

    Open Library

  7. Click Upgrade in the Open library window and the Library Upgrade progress window displays.

    Library Upgrade

    The function block library opens and is located in the Global Libraries pane of the Siemens TIA Portal.

    Global Libraries

For additional information, refer to the Siemens TIA Portal information and Third Party Documentation.

Library Compatibility: The function block library for accessing the TeSys™ island via PROFIBUS DP and PROFINET IO bus couplers are compatible with Siemens TIA Portal V15. All function blocks and data blocks included in the library are compiled for non-optimized access. For execution, the function blocks in the library require the availability of certain System Function Blocks on the SIMATIC PLCs. For a detailed description of these dependencies, refer section Function Block Library.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.