DOCA0272EN-00

Avatar Energy Management

Function block profile

Function block type

Avatar Generic function block.

Type of data access

Cyclic (write) and acyclic (read).

Intended use

All Load, Application and Device avatars. For the Device avatars “Analog I/O” and “Digital I/O” the data can be retrieved but will only contain default values as these avatars do not support this functionality.

Functionality

The Avatar Energy function block returns the status of the energy data of the specified avatar.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.