DOCA0272EN-00

System Time

Function block profile

Function block type

System avatar function block.

Type of data access

Acyclic (read/write).

Intended use

System avatar (Bus coupler).

Functionality

The System Time function block reads and writes the system time of the Bus coupler. Write command has higher priority.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.