DOCA0272EN-00

PN_SystemWriteCmds (PROFINET IO)

The following tables give information about the parameters of the function block interface.

Inputs

Input

Data Type

Description

Variable Category

i_xEnable

BOOL

Activates the function block processing. Cyclic data will be read/written to the hardware IO interface.

Function block control

i_xAcyclicBusy

BOOL

Can be used to block the acyclic execution if acyclic communication of another function block is active.

Function block control

i_xExecute

BOOL

Starts an acyclic request on a rising edge.

Function block control

i_uiNoConfAvatar

UINT

Used to parameterize the number of configured avatars to define the length of the data, which needs to be written. Minimum value is 0 (only Bus coupler) and maximum value is 20.

Function block control

i_udtAcyclicWriteCmds

UDT_SystemWriteCmds

This is a structure of acyclic system write data, which includes reset commands and energy data of the system and all avatars. For detailed information about the structure of this UDT, see UDT_SystemWriteCmds.

Acyclic data

i_hwSubmHWID

HW_IO

Must correspond to the hardware identifier of the acyclic submodule of the related avatar to be able to execute the acyclic communication.

Communication parameter

Outputs

Output

Data Type

Description

Variable Category

q_xActive

BOOL

If this output is set to TRUE, the Avatar function block is enabled, or an acyclic request is busy.

Function block status

q_xError

BOOL

If this output is set to TRUE, a detected error occurred while executing the Avatar function block. For detailed information about the detected error, see the value of the Error ID.

Function block status

q_dwErrorID

DWORD

The Error ID shows detailed information about the detected error that occurred. Possible values are shown in the table below.

Function block status

q_dwAcyclicStatus

DWORD

The Acyclic status provides detailed information about the acyclic fieldbus communication, including detected error details. For detailed information about the status values, see Function Block Library.

Function block status

q_xAcyclicBusy

BOOL

If this output is set to TRUE, an acyclic request is still busy.

Function block status

Status and error codes from ConstTeSysIsland

Member name

Used by the function block

Cdw_ErrNoMsg

Yes

Cdw_ErrInternal

Yes

Cdw_ErrInvalidCycInAddr

No

Cdw_ErrInvalidHwid

Yes

Cdw_ErrInvalidNumOfAvatars

Yes

Cdw_ErrReadCycIn

No

Cdw_ErrReadAcycData1

No

Cdw_ErrReadAcycData2

No

Cdw_ErrWriteAcycData

Yes

Cdw_StsReadAcycData1Compl

No

Cdw_StsReadAcycData2Compl

No

Cdw_StsWriteAcycDataCompl

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.