DOCA0272EN-00

Data Access

As previously stated, the function blocks use both cyclic and acyclic communication mechanisms to retrieve data from and send data to the TeSys™ island, depending on their functionality.

The following sections give an overview of how these two communication mechanisms can be controlled at the function block interface, what status information about the communication is available, and what parameters are involved to configure data access.

Variables to control cyclic communication

Function block status

Variables to control the Avatar communication

Avatar status

Variables to control acyclic communication

Results of acyclic communication

Parameters for cyclic and acyclic communication

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.