DOCA0272EN-00

UDT_SystemEnergy2

The SystemEnergy2 UDT is used to transfer the acyclic energy and power data of the System avatar. The interfaces of the PN_SystemEnergy and DP_SystemEnergy function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

VSwellRecordReg1

STRUCT

See Struct VSwellRecordRegX.

VSwellRecordReg2

STRUCT

See Struct VSwellRecordRegX.

VSwellRecordReg3

STRUCT

See Struct VSwellRecordRegX.

VSwellRecordReg4

STRUCT

See Struct VSwellRecordRegX.

VSwellRecordReg5

STRUCT

See Struct VSwellRecordRegX.

VSwellCnt

UINT

Voltage swell counter value.

TotActPow

DINT

Total active power for the system. (Unit: W)

MaxTotActPow

DINT

Maximum value of the active power for the system. (Unit: W)

MaxTotActPowTimestamp

DTL

Date and time when the maximum active power value was recorded.

TotReactPower

DINT

Total reactive power for the system. (Unit: VAR)

MaxTotReactPow

DINT

Maximum value of the reactive power for the system. (Unit: VAR)

MaxTotReactPowTimestamp

DTL

Date and time when the maximum reactive power value was recorded.

TruePowFact

USINT

True power factor value.

MinTruePowFact

USINT

True minimum power factor value.

MaxTruePowFact

USINT

True maximum power factor value.

MinTruePowFactTimestamp

DTL

Date and time when the minimum true power factor value was recorded.

MaxTruePowFactTimestamp

DTL

Date and time when the maximum power factor value was recorded.

TotActEnergy

UDINT

Total active energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: Wh)

TotReactEnergy

UDINT

Total reactive energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: VARh)

Struct VSwellRecordRegX

Element

Data Type

Description

uiMagnitude

UINT

Magnitude of the voltage register.

dtlStartDate

DTL

Start timestamp of the voltage register.

dtlStopDate

DTL

Stop timestamp of the voltage register.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.