DOCA0272EN-00

Conveyor, One Direction

Function block profile

Function block type

Avatar Control function block.

Type of data access

Cyclic (read/write) and acyclic (read).

Intended use

Application avatar “Conveyor, One Direction“.

Functionality

The Conveyor One Direction function block is used to manage a conveyor in one direction.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.