DOCA0272EN-00

Library compatibility

The function block library described in this document has been developed for the Siemens® TIA Portal V15. It should be compatible with any Siemens SIMATIC S7-1200 or S7-1500 series PLCs that meet the PLC requirements (see below).

The library should be compatible with any firmware version of TeSys™ island and any DTM library version for TeSys™ island sharing the same major and minor version (at the time of writing this documentation, version 2.2.x)

All elements within the library (function blocks and data blocks) are configured to use non-optimized data access.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.