DOCA0272EN-00

Power Interface Module, Asset Management

Function block profile

Function block type

Device function block.

Type of data access

Acyclic (read).

Intended use

Power Interface Module device.

Functionality

The Power Interface Module, Asset Management function block returns the status of the acyclic asset management data of the specified device.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.