DOCA0272EN-00

System Avatar Function Blocks

The System avatar represents the whole island as a system. The System avatar allows the setting of the network configuration, and it computes island-level data. The function blocks of this category provide access to the various functionalities of the System avatar as well as its Diagnostic, Energy, and Asset Management Data. The function blocks of this category are contained in the folders “DP_System” (PROFIBUS DP) and “PN_System” (PROFINET IO) of the library respectively.

System avatar function blocks use a combination of cyclic input and output data as well as acyclic read and write requests, depending on the functionality of the individual function block.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.