DOCA0272EN-00

Device Asset Management Function Blocks

Asset Management Data supplements the data of the System avatar and the individual Device, Load, and Application avatars. Asset Management Data of the island devices can be accessed through the Device Asset Management function blocks. For each type of device, an individual function block has been created. Starters and SIL* Starters share a common implementation, as do Digital and Analog I/O modules. These function blocks can be found in the folders “DP_Devices” and “PN_Devices”. The function blocks must be instantiated for each device that the Asset Management data is retrieved for.

Device Asset Management function blocks only use acyclic read requests.

NOTE: The devices of the TeSys™ island are represented in the slots starting at number 101 on the TeSys™ island bus device for both PROFINET IO and PROFIBUS DP.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.