DOCA0272EN-00

UDT_Energy

The Energy UDT is used to transfer the acyclic energy data of an avatar, like power and active/reactive energy information. The interfaces of the PROFINET IO and PROFIBUS DP generic energy avatar function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

TotActPower

DINT

Total active power for the avatar. (Unit: W)

MaxTotActPow

DINT

Maximum value of the active power value for the avatar (Unit: W)

MaxTotActPowTimestamp

DTL

Date and time when the maximum active power value was recorded.

TotReactPower

DINT

Total reactive power value of the avatar (Unit: VAR)

MaxTotReactPow

DINT

Maximum value of the reactive power value for the avatar (Unit: VAR)

MaxTotReactPowTimestamp

DTL

Date and time when the maximum reactive power value was recorded.

TruePowFact

USINT

True power factor value.

MinTruePowFact

USINT

Minimum value of the true power factor.

MaxTruePowFact

USINT

Maximum value of the true power factor.

MinTruePowFactTimestamp

DTL

Date and time when the minimum true power factor was recorded.

MaxTruePowFactTimestamp

DTL

Date and time when the maximum value of the true power factor was recorded.

TotActEnergy

UDINT

Total active energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: Wh)

TotReactEnergy

UDINT

Total reactive energy value for all avatars in the system with Energy Monitoring Enabled. (Unit VARh)

ToU_TotActEnergyCh1

UDINT

Channel 1: ToU (Time of Use) total active energy value.

ToU_TotActEnergyCh2

UDINT

Channel 2: ToU (Time of Use) total active energy value.

ToU_TotActEnergyCh3

UDINT

Channel 3: ToU (Time of Use) total active energy value.

ToU_TotActEnergyCh4

UDINT

Channel 4: ToU (Time of Use) total active energy value.

ToU_TotReactEnergyCh1

UDINT

Channel 1: ToU (Time of Use) total reactive energy value.

ToU_TotReactEnergyCh2

UDINT

Channel 2: ToU (Time of Use) total reactive energy value.

ToU_TotReactEnergyCh3

UDINT

Channel 3: ToU (Time of Use) total reactive energy value.

ToU_TotReactEnergyCh4

UDINT

Channel 4: ToU (Time of Use) total reactive energy value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.