DOCA0272EN-00

UDT_WRREC

The WRREC UDT is used to store status information of an acyclic write request internally.

Elements

Element

Data Type

Description

xQ_RTrig

BOOL

Rising edge result, to transfer data to function block variables.

qxDone

BOOL

Acyclic write request result is DONE.

qxBusy

BOOL

Acyclic write function is busy.

qxError

BOOL

Acyclic write request ends with ERROR.

qdwStatus

DWORD

Status result of acyclic write function.

ixStartWrite

BOOL

Enable/Start acyclic write function.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.