DOCA0272EN-00

UDT_SystemDiag

The SystemDiag UDT is used to transfer the acyclic diagnostic data of the system. The interfaces of the PROFINET IO and PROFIBUS DP SystemDiag avatar function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

CntErrComm

UINT

Number of detected errors for the fieldbus communication.

CntAllAlarms

UINT

Number of detected alarms for the system.

CntSystemEvt

UINT

Number of detected minor events for the system.

EvtRecReg1

STRUCT

Information on a detected minor event – register 1. See Struct EvtRecRegX.

EvtRecReg2

STRUCT

Information on a detected minor event – register 2. See Struct EvtRecRegX.

EvtRecReg3

STRUCT

Information on a detected minor event – register 3. See Struct EvtRecRegX.

EvtRecReg4

STRUCT

Information on a detected minor event – register 4. See Struct EvtRecRegX

EvtRecReg5

STRUCT

Information on a detected minor event – register 5. See Struct EvtRecRegX.

SILStopMsgGrp1

STRUCT

Status for SIL Stop 0* function of SIL group 1. See Struct SILStopMsgX.

SILStopMsgGrp2

STRUCT

Status for SIL Stop 0 function of SIL group 2. See Struct SILStopMsgX.

SILStopMsgGrp3

STRUCT

Status for SIL Stop 0 function of SIL group 3. See Struct SILStopMsgX.

SILStopMsgGrp4

STRUCT

Status for SIL Stop 0 function of SIL group 4. See Struct SILStopMsgX.

SILStopMsgGrp5

STRUCT

Status for SIL Stop 0 function of SIL group 5. See Struct SILStopMsgX.

SILStopMsgGrp6

STRUCT

Status for SIL Stop 0 function of SIL group 6. See Struct SILStopMsgX.

SILStopMsgGrp7

STRUCT

Status for SIL Stop 0 function of SIL group 7. See Struct SILStopMsgX.

SILStopMsgGrp8

STRUCT

Status for SIL Stop 0 function of SIL group 8. See Struct SILStopMsgX.

SILStopMsgGrp9

STRUCT

Status for SIL Stop 0 function of SIL group 9. See Struct SILStopMsgX.

SILStopMsgGrp10

STRUCT

Status for SIL Stop 0 function of SIL group 10. See Struct SILStopMsgX.

Struct EvtRecRegX

Element

Data Type

Description

DTL

DTL

TIA timestamp format

FFFF

WORD

Detected minor event identifier.

0000: No Detected Minor Event.

0001: No module in the island.

0002: Number of physical devices detected in the island is beyond the limit allowed.

0003: Modules mismatch.

0004: Island control power supply voltage fluctuation.

Struct SILStopMsgX

Element

Data Type

Description

SILGrpNotInSysConf

BOOL

SIL Group not present in system configuration

Reserved

BOOL

SIL Group impacted by Avatar Device event

SILCmdRecSILStarterNotOpen

BOOL

SIL Group stop command received; SIL starters not open yet

SILCmdOkSILStarterOpened

BOOL

SIL Group stop command successfully issued; all SIL starters are open

SILCmdTo1Terminal

BOOL

SIL Group stop command issued to only 1 SIL interface module (SIM) input channel (jumper or SIM input wiring is causing an issue) but SIL starters did successfully open

NormalOperation

BOOL

Normal operation, SIL starters can be open or closed

<Reserved>

BOOL

Byte-filler

<Reserved>

BOOL

Byte-filler

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.