DOCA0272EN-00

UDT_PredictiveAlarmMessages

The PredictiveAlarmMessages UDT is used as a template when importing the predictive alarm status messages from SoMove™ software into the TIA Portal. This UDT contains the predictive alarm status messages for one avatar. See the TeSys™ island Quick Start Guide for PROFINET and PROFIBUS Applications, document number 8536IB1916 for more details on importing predictive alarm status messages.

Elements

Element

Data Type

Description

PAStatusMessage0

STRING[150]

Message associated with Predictive Alarm Bit 0

PAStatusMessage1

STRING[150]

Message associated with Predictive Alarm Bit 1

PAStatusMessage2

STRING[150]

Message associated with Predictive Alarm Bit 2

PAStatusMessage3

STRING[150]

Message associated with Predictive Alarm Bit 3

PAStatusMessage4

STRING[150]

Message associated with Predictive Alarm Bit 4

PAStatusMessage5

STRING[150]

Message associated with Predictive Alarm Bit 5

PAStatusMessage6

STRING[150]

Message associated with Predictive Alarm Bit 6

PAStatusMessage7

STRING[150]

Message associated with Predictive Alarm Bit 7

PAStatusMessage8

STRING[150]

Message associated with Predictive Alarm Bit 8

PAStatusMessage9

STRING[150]

Message associated with Predictive Alarm Bit 9

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.