DOCA0272EN-00

UDT_Diagnostic

The Diagnostic UDT is used to transfer the acyclic diagnostic data of an avatar, like Irms, alarm and trip information. The interfaces of the PROFINET IO and PROFIBUS DP generic diagnostic avatar function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

MaxAvgIRMS

UDINT

Maximum average Irms current value.

MaxAvgIRMSTImeStamp

DTL

Date and time when the maximum average value of the Irms current was recorded.

IRMSPhase1

UDINT

Value of the phase L1 Irms. (Unit: mA).

IRMSPhase2

UDINT

Value of the phase L2 Irms. (Unit: mA).

IRMSPhase3

UDINT

Value of the phase L3 Irms. (Unit: mA).

AlarmCnt

STRUCT

Alarm counters. See Struct AlarmCnt.

TripCnt

STRUCT

Trip counters. See Struct TripCnt.

TripRecReg1

STRUCT

Record 1 of a trip event. See Struct TripRecRegX.

TripRecReg2

STRUCT

Record 2 of a trip event. See Struct TripRecRegX.

TripRecReg3

STRUCT

Record 3 of a trip event. See Struct TripRecRegX.

TripRecReg4

STRUCT

Record 4 of a trip event. See Struct TripRecRegX.

TripRecReg5

STRUCT

Record 5 of a trip event. See Struct TripRecRegX.

Struct AlarmCnt

Element

Data Type

Description

ThermOverload

UInt

Counter of advisories related to thermal overload protection.

Jam

UInt

Counter of advisories related to jam protection.

Undercurrent

UInt

Counter of advisories related to undercurrent protection.

Overcurrent

UInt

Counter of advisories related to overcurrent protection.

IPhaseUnbal

UInt

Counter of advisories related to phase unbalance protection.

GroundCurrent

UInt

Counter of advisories related to ground current protection.

Overheat

UInt

Counter of motor overheat events.

AllAlarms

UInt

Counter of advisories related to protections.

Struct TripCnt

Element

Data Type

Description

ThermOverload

UInt

Counter of trips related to thermal overload protection.

Jam

UInt

Counter of trips related to jam protection.

Undercurrent

UInt

Counter of trips related to undercurrent protection.

LongStart

UInt

Counter of trips related to long start protection.

Overcurrent

UInt

Counter of trips related to overcurrent protection.

Overheat

UInt

Counter of motor overheat trip events.

Stall

UInt

Counter of trips related to stall protection.

IPhaseUnbal

UInt

Counter of trips related to phase unbalance protection.

PhaseConfT

UInt

Counter of trips related to phase configuration protection.

GroundCurrent

UInt

Counter of trips related to ground current protection.

PhaseReversal

UInt

Counter of trips related to phase reversal protection.

CurrentPhaseLoss

UInt

Counter of trips related to phase loss protection.

AllTrips

UInt

Counter of trips related to protections.

Struct TripRecRegX

Element

Data Type

Description

DTL

DTL

TIA timestamp format

TTTT

WORD

Trip event identifier

0000—No Detected Event

0001—Thermal Overload

0002—Motor Overheat

0003—Jam

0004—Undercurrent

0005—Long Start

0006—Overcurrent

0007—Stall

0008—Ground Current

0009—Current Phase Reversal

0010—Phase Configuration

0011—Current Phase Unbalance

0012—Current Phase Loss

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.