DOCA0272EN-00

UDT_SystemEnergy1

The SystemEnergy1 UDT is used to transfer the acyclic voltage energy data of the System avatar. The interfaces of the PN_SystemEnergy and DP_SystemEnergy function blocks contain this UDT as a parameter.

Elements

Element

Data Type

Description

VrmsAverg

UINT

Average Vrms voltage on three phases. (Unit: V)

VrmsMaxAvg

UINT

This register indicates maximum voltage the avatar has measured in its lifetime. (Unit: V)

VtimeMaxAvg

DTL

Timestamp of maximum average.

VrmsPhase1

UINT

Average Vrms voltage between L1 and neutral. (Unit: V)

VrmsPhase2

UINT

Average Vrms voltage between L2 and neutral. (Unit: V)

VrmsPhase3

UINT

Average Vrms voltage between L3 and neutral. (Unit: V)

VrmsL1L2

UINT

Average Vrms voltage between L1 and L2. (Unit: V)

VrmsL2L3

UINT

Average Vrms voltage between L2 and L3. (Unit: V)

VrmsL3L1

UINT

Average Vrms voltage between L3 and L1. (Unit: V)

VUnbalPerc

USINT

Unbalance voltage in percent (%).

VUnbalMax

USINT

Maximum unbalance voltage in percent (%).

VtimeUnbalMax

DTL

Date and time of maximum unbalance voltage.

PhaseSequ

Byte

Phase sequence (ABC or ACB).

Frequency

USINT

Main power voltage frequency (line frequency as measured on phase 1). (Unit: Hz)

VDipRecordReg1

STRUCT

Voltage Dip record register 1. See Struct VDipRecordRegX.

VDipRecordReg2

STRUCT

Voltage Dip record register 2. See Struct VDipRecordRegX.

VDipRecordReg3

STRUCT

Voltage Dip record register 3. See Struct VDipRecordRegX.

VDipRecordReg4

STRUCT

Voltage Dip record register 4. See Struct VDipRecordRegX.

VDipRecordReg5

STRUCT

Voltage Dip record register 5. See Struct VDipRecordRegX.

VDipCnt

UINT

Voltage dip counter value.

Struct VDipRecordRegX

Element

Data Type

Description

uiMagnitude

UINT

Magnitude of the voltage register.

dtlStartDate

DTL

Start timestamp of the voltage register.

dtlStopDate

DTL

Stop timestamp of the voltage register.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.