DOCA0272EN-00

Digital I/O

Function block profile

Function block type

Avatar Control function block.

Type of data access

Cyclic (read/write).

Intended use

Device avatar “Digital I/O”.

Functionality

The Digital l/O function block provides information about the Digital I/O avatar with four inputs and two outputs.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.