DOCA0272EN-00

How to Add a New PLC

To add a new PLC to your project, follow these steps:

  1. Open an existing project.

  2. Click Add new device. Click Controllers and navigate to your PLC, then select OK.

    Add New Device

  3. The new PLC appears in the Topology view. Select the Network View to view and assign the TeSys™ island device.

    Network View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.