DOCA0272EN-00

Resistor

Function block profile

Function block type

Avatar Control function block.

Type of data access

Cyclic (read/write) and acyclic (read).

Intended use

Load avatar “Resistor“.

Functionality

The Resistor function block is used to manage a resistive load.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.