DOCA0272EN-00

Installing the Siemens TIA Portal

The software package for Siemens TIA Portal Openness must be installed along with Siemens TIA Portal before the CAx data import feature of the Siemens TIA Portal is available for use. This package is available for free. Siemens TIA Portal V15.1 package is automatically installed by default.

For Siemens TIA Portal and TIA Portal Openness system requirements and detailed instructions about how to install them, refer to Third Party Documentation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.