DOCA0272EN-00

PN_SystemControl (PROFINET IO)

The following tables give information about the parameters of the function block interface.

Inputs

Input

Data Type

Description

Variable Category

i_xEnable

BOOL

Activates the function block processing. Cyclic data will be read/written to the hardware IO interface.

Function block control

i_xResetSystem

BOOL

If this input is set to TRUE, the system is reset.

Cyclic data

i_hwStartAddress

Variant

Must correspond to the first address of the cyclic input submodule address range of the related avatar to be able to execute cyclic read communication

Communication parameter

In/Out

InOut

Data Type

Description

Variable Category

iq_hwQBAddress

Byte

Must correspond to the address of the cyclic output submodule to be able to execute cyclic write communication

Communication parameter

Outputs

Output

Data Type

Description

Variable Category

q_xActive

BOOL

If this output is set to TRUE, the Avatar function block is enabled, or an acyclic request is busy.

Function block status

q_xError

BOOL

If this output is set to TRUE, a detected error occurred while executing the Avatar function block. For detailed information about the detected error, see the value of the Error ID.

Function block status

q_dwErrorID

DWORD

The Error ID shows detailed information about the detected error that occurred. Possible values are shown in the table below.

Function block status

q_xSystemOperat

BOOL

If this output is set to TRUE, the System avatar is in Operational mode. For detailed information on machine states, refer to the TeSys island – System, Installation, and Operation Guide document.

Cyclic data

q_xDegradedMode

BOOL

If this output is set to TRUE, the System avatar is in Degraded mode.

Cyclic data

q_xMinorEvent

BOOL

If this output is set to TRUE, the System avatar is in detected Minor Event mode.

Cyclic data

q_xPreOperat

BOOL

If this output is set to TRUE, the System avatar is in Preoperational mode.

Cyclic data

q_xForceMode

BOOL

If this output is set to TRUE, the System avatar is in Force mode.

Cyclic data

q_xTestMode

BOOL

If this output is set to TRUE, the System avatar is in Test mode.

Cyclic data

Status and error codes from ConstTeSysIsland

Member name

Used by the function block

Cdw_ErrNoMsg

Yes

Cdw_ErrInternal

No

Cdw_ErrInvalidCycInAddr

Yes

Cdw_ErrInvalidHwid

No

Cdw_ErrInvalidNumOfAvatars

No

Cdw_ErrReadCycIn

Yes

Cdw_ErrReadAcycData1

No

Cdw_ErrReadAcycData2

No

Cdw_ErrWriteAcycData

No

Cdw_StsReadAcycData1Compl

No

Cdw_StsReadAcycData2Compl

No

Cdw_StsWriteAcycDataCompl

No

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.