DOCA0272EN-00

Power Interface – with I/O (control)

Function block profile

Function block type

Avatar Control function block.

Type of data access

Cyclic (read/write) and acyclic (read).

Intended use

Load Avatar “Power Interface – with I/O”.

Functionality

The Power Interface with I/O function block is used to monitor current and control an external power device, such as a solid-state relay, soft starter, or variable speed drive.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.